Gainspan GS1500M module security mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gainspan GS1500M module security mode?

1,285件の閲覧回数
danielchai
Senior Contributor I

Hi All,

I am working on the TWR-K60F120 with GS1500M tower board.

In the demo code, I enable the DEMOCFG_SECURITY to "wpa2" and set the DEMOCFG_PASSPHRASE to "123456".

But when I connect the wifi using my PC, it does not ask me for the password. PC can connect to the wifi automatically without asking for password.

Any ideas about this?

Thank you.

-Daniel

0 件の賞賛
返信
2 返答(返信)

1,188件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Daniel Chai,

      Which demo code do you modify? TWR-WiFi-GS1500M_SER2WiFi_SC?

Best regards?

Jing

0 件の賞賛
返信

1,188件の閲覧回数
danielchai
Senior Contributor I

Hi Jing,

Actually, I use the demo code httpsrv which is based on the MQX.

Thank you.

-Daniel

0 件の賞賛
返信