GPIO outputs affected by wdog?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO outputs affected by wdog?

Jump to solution
1,601 Views
gsosnow
Contributor II

For the  MK22FN512CBP12R I want to configure some gpios as outputs to control some external chips. My question is if a watchdog reset occurs will these gpios revert to inputs? If so, is there any way to prevent this from occurring, since reverting to inputs could affect the control and state of the external chips?

0 Kudos
Reply
1 Solution
1,548 Views
mjbcswitzerland
Specialist V

George

A watchdog reset causes the GPIOs to be set to their default states - most as inputs or default peripheral functions.

If you want the states to be held in a particular state when this happens you will need to use external pullup and pull-downs to control the required state.

Regards

Mark

View solution in original post

0 Kudos
Reply
1 Reply
1,549 Views
mjbcswitzerland
Specialist V

George

A watchdog reset causes the GPIOs to be set to their default states - most as inputs or default peripheral functions.

If you want the states to be held in a particular state when this happens you will need to use external pullup and pull-downs to control the required state.

Regards

Mark

0 Kudos
Reply