GPIO in L-series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO in L-series

2,420 Views
Markon
Contributor II

Hi,

I'm preparing project with MKL16Z64VLH4 and I have questions:

1. May I activate interrupt on every port A, B, C, D, E?

2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

Labels (1)
3 Replies

2,232 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Mar Kon

Q1. May I activate interrupt on every port A, B, C, D, E?

A1: No, Kinetis L series does not support all ports interrupt.

Q2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

A2: You can reference chapter "Interrupt channel assignments" in reference manual. There is a table which tell you which port can support GPIO interrupt and which port can only support single interrupt.

Hope my reply can help you.

Best Regards

Paul

2,232 Views
Markon
Contributor II

Thank you for your answer.

May I ask you about reference manual for MKL16Z64VLH4 because there isn't any connected with this processor on freescale webside?

0 Kudos
Reply

2,232 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mar Kon,

    Reference manual for MKL16Z64VLH4 will be recently launched, please pay aattention to the website.

    Best regards!

Jing