GPIO group configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO group configuration

ソリューションへジャンプ
2,554件の閲覧回数
gschelotto
Contributor V

Hi,

I have to configure more than 40 independent GPIOs on MKE02Z64VLH4 mcu. Currently I'm using PE-KDS 3.0 to configure each port (input/output, initial value and so on) but I wonder if there is other (agile) way to do it.Any hints?

Thanks in advance,

gaston

0 件の賞賛
返信
1 解決策
2,403件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please check the GPIO_LDD component, which could set multiple pins function in bit fields.

2016-04-07_14-00-00.jpg

Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,404件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please check the GPIO_LDD component, which could set multiple pins function in bit fields.

2016-04-07_14-00-00.jpg

Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,403件の閲覧回数
gschelotto
Contributor V

Ma Hui, You were right. I've added scattered GPIOs using different Bit fields in GPIO_LDD component. This is okay for me.

thanks,
gaston

0 件の賞賛
返信
2,403件の閲覧回数
gschelotto
Contributor V

Hi Ma Hui,

Thanks, I can see GPIO_LDD is useful when data bus implementation is needed. However in my case I have to configure lot of scattered GPIOs and I have to control them individually. So far I've been doing it with BitIO_LDD but configuring more than 40 GPIOs using this component is a bit tedious. Any suggestion without PE?

regards,

gaston

0 件の賞賛
返信