GPIO Open Drain: Schematic?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Open Drain: Schematic?

Jump to solution
4,059 Views
belskyc
Contributor III

Hello,

 

In the Kinetis K60 uP, the general-purpose-input-output (GPIO) port register PORTx_PCRn, bit ODE called "Open Drain Enable" allows the port to be configured with an "Open Drain Output".  Could anyone please explain to me what the significance of Open-Drain is?  Schematically speaking, what does the port look like with the "Open Drain" enabled vs. disabled?  I'm trying to understand when an application would want an Open-Drain output vs. a non-open-drain. 

 

Thanks and regards,

~

0 Kudos
Reply
1 Solution
2,819 Views
mjbcswitzerland
Specialist V

Hi

 

I think that a standard open-drain description contains this information:

http://en.wikipedia.org/wiki/Open_collector

 

Regards

 

Mark

 

View solution in original post

0 Kudos
Reply
1 Reply
2,820 Views
mjbcswitzerland
Specialist V

Hi

 

I think that a standard open-drain description contains this information:

http://en.wikipedia.org/wiki/Open_collector

 

Regards

 

Mark

 

0 Kudos
Reply