GPIO Open Drain: Schematic?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Open Drain: Schematic?

ソリューションへジャンプ
4,077件の閲覧回数
belskyc
Contributor III

Hello,

 

In the Kinetis K60 uP, the general-purpose-input-output (GPIO) port register PORTx_PCRn, bit ODE called "Open Drain Enable" allows the port to be configured with an "Open Drain Output".  Could anyone please explain to me what the significance of Open-Drain is?  Schematically speaking, what does the port look like with the "Open Drain" enabled vs. disabled?  I'm trying to understand when an application would want an Open-Drain output vs. a non-open-drain. 

 

Thanks and regards,

~

0 件の賞賛
返信
1 解決策
2,837件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

I think that a standard open-drain description contains this information:

http://en.wikipedia.org/wiki/Open_collector

 

Regards

 

Mark

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,838件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

I think that a standard open-drain description contains this information:

http://en.wikipedia.org/wiki/Open_collector

 

Regards

 

Mark

 

0 件の賞賛
返信