GCC compiler in CW10.1 optimized for M4?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GCC compiler in CW10.1 optimized for M4?

1,883 次查看
tmf
Contributor I

Is it aware of optimizations for M4? It seems not to be......

 

would you not expect

 

static inline int MULSHIFT32(register int x, register int y)
{
  return (((Word64)x*(Word64)y)>>32);
}

 

SMULL  R3, R2, R1, R0
MOVS  R0, R2

 

to be compiled to a couple op-codes?

 

Richard.

0 项奖励
回复
3 回复数

1,579 次查看
MikeAdv
Contributor III

This is along the lines of my question as well.

 

I want to use multiply two 32 bit numbers and get the top 32 bits of the result.  How do I do that most efficiently from C?

 

 

0 项奖励
回复

1,579 次查看
eli_hughes
Contributor V

Look in the CMSIS DSP libraries.   I believe all you have to do is cast to a "long long" for the result and bit shift

0 项奖励
回复

1,579 次查看
MikeAdv
Contributor III

I have tried this and it doesn't seem to work.

 

int my_mult(int a, int b) { int c; c = ((long long)a*b) >> 32; return c;}

 

This function generates the following assembly:

 

          my_mult:1fff0238:   push {r3-r4}41         return c;1fff023a:   asr r12,r1,#asr #311fff023e:   umull r2,r3,r0,r11fff0242:   mla r3,r0,r12,r31fff0246:   asrs r4,r0,#311fff0248:   mla r3,r4,r1,r31fff024c:   cpy r0,r342        }

 

No smull there.  Furthermore, I don't understand why it is using an unsigned multiply (umull) when I'm using signed ints.

 

I'm not familiar with the CMSIS library.  I'll try to figure that out.

0 项奖励
回复