Future availability of MK22FN512VMP12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Future availability of MK22FN512VMP12

1,264 次查看
pulsatrixp1
Contributor III

The product brief of MK22 family indicates that the MK22FN512VMP12 part will not be available soon, but in the webpage it is not indicated that is not recommended for new designs, and distributors have stock. Is it safe to use this part for a new design in terms that it will be supported and manufactured continuously afterwards?

标签 (1)
0 项奖励
回复
3 回复数

1,122 次查看
pulsatrixp1
Contributor III

Hi Kerry,

Thank you for your reply. I cannot find back the document where I saw it at the moment. 

I have anyway selected the MK22FN1M0AVMC12 for my application, compromising a little on size (8*8 instead of 5*5) in order to use the extended flash memory.

Best Regards,

Ivan

0 项奖励
回复

1,122 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pulsatrix P1,

  Yes, you can select MK22FN1M0AVMC12, it is also the hot product.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,122 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pulsatrix P1,

   

   Could you give me a screenshot in the K22 PB which says : MK22FN512VMP12 part will not be available soon?

   I didn't find this description in the K20 PB.

   As I know, MK22FN512VMP12 is still the kinetis hot product,  from the MK22FN512VMP12 part details:

https://www.nxp.com/webapp/search.partparamdetail.framework?PART_NUMBER=MK22FN512VMP12&buyNow=true&f... 

   You can get that this part  Life Cycle Description is PRODUCT RAPID GROWTH, Application/Qualification Tier is 10-YEARS APPLICATION LIFE.

  So, you can use it in your new design.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------