Chip: Freescale MK10DN512ZVLL10-4N30D (Kinetis K10)
Issue: ADC module/Peripheral conversions slowing down after 30-90 days and subsequently stalling/damaged permanently.
No of chips affected/damaged: 20 Nos.
Core Clock: 100Mhz
Bus Clock: 50MHz
ADC Operating Frequency: 50/8=6.25MHz
Hardware Average: No/Disabled
Long Sample: Yes
Long Sample clocks: Extra cycles
Total ADCs connected: 11
No. of Differential channels connected: 4
ADC Resolution :16-bit
No. of Single-ended channels connected: 7
ADC Resolution :16-bit
In-depth Problem:
Attached is the Code* for Core clock, ADC clock & ADC reading.
Also attached is the schematic* for reference.
*Only ADC section.other details/specifics taken out
Please acknowledge, analyze, diagnose & suggest what is going wrong/what is causing ADC to damage/any corrections in code or schematic.Any suggestions will be appreciated.
Brij
@titan99bijou did you get the solution or root cause of the problem ? I also have the similar issue and not getting any clue even with failure analysis by NXP.
 
					
				
		
 xiangjun_rong
		
			xiangjun_rong
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		From your phenomenon, it is difficult to get the root cause. But I have checked your code, it seems that your code has issue.
For example:
LDR R0,=SIM_BASE
LDR R1,[R0,#SIM_SCGC6_OFS]
MOV R2,#(1<<27)
ORR R1,R1,R2
STR R1,[R0,#SIM_SCGC6_OFS]
I do not think that the "MOV R2,#(1<<27)" is correct, as you know that the immediate value should less than 16 bits for MOV instruction so that the MOV can generate 32 bits coding. I have use the CW to compile the instruction, I get error for the above instruction. I think your assembly compiler has issue, can you tell me the assembly compiler you are using?
If you do want to use assembly language to develop code, can you switch to CW tools?
BR
Xiangjun rong
Hi Rong,
Thanks for your views & time spent there. But seems the instruction is behaving as desired. Am using a Keil 4 Assembler & attached is the snapshot of the debugger at that instruction.It can been seen that the MOV R2,#(1<<27) shifts 1, 27 bits to the Left thereby activating the ADC clock.
Can some1 please check my Core,Bus & ADC Clocks are in range & within specifications?
 
					
				
		
Actually, the Cortex M4 instructions allow for 'somewhat more general' fixed values in addition to 'immediate 16 bits'.
From DUI0553A_cortex_m4_dgug.pdf:
Constant
You specify an Operand2 constant in the form:
#constant
where constant can be these (or for MVN [move negate] their inverse):
• any constant that can be produced by shifting an 8-bit value left by any number of bits
within a 32-bit word
• any constant of the form 0x00XY00XY
• any constant of the form 0xXY00XY00
• any constant of the form 0xXYXYXYXY.
How individual assemblers create the syntax to implement these different forms is probably 'implementation dependent'.