Freescale Kinetis K20 based MK20FN1M0VMD12 reset state question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freescale Kinetis K20 based MK20FN1M0VMD12 reset state question

跳至解决方案
2,285 次查看
sherry_zahid
Contributor III

Hi,

I am working with MK20FN1M0VMD12 K20 based processor. I am looking at the default pin assignment in the datasheet, for example the pin "PTD11" says "disabled" under default. I understand that this means the pin will be disabled on reset. How does it behave exactly? Will PTD11 be pulled up/down? What exactly does "disabled" mean? Will I need to put an external (current limiting or pull up) resistor to this pin for microcontroller safety?

Thanks for your time,

Sherry

0 项奖励
回复
1 解答
2,163 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Sherry

Disable means high-impedance. So you have leave this pin floating.

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

2 回复数
2,164 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Sherry

Disable means high-impedance. So you have leave this pin floating.

Hope my reply can help you.

Best Regards

Paul

2,163 次查看
sherry_zahid
Contributor III

Thanks Paul

0 项奖励
回复