FreeMaster interface usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMaster interface usage

3,922件の閲覧回数
diego_ambroggi
Contributor I

Hi everybody

I tried to use FreeMaster interface in my project but it doesn't work.

I Created component in Processor Expert choosing UART0 and I called "FMSTR1_Poll()" in main loop.

I can't find examples for this. 

Have some tips for me?

Thanks in advance

ラベル(2)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

3,734件の閲覧回数
marciol_carleto
Contributor I

Hi,

I´m facing the same problem here, the difference is that I`m using  S9KEAZ128AVLH instead.

I have tried using Freemaster PEx component on UART1 (PTC6 and PTC7 pins communicating thru RS232 to my PC), initialized UART1 and called FMSTR_Init(); before the main loop and inside the main loop I have called FMSTR_Recorder(); and FMSTR_Poll(); but I wasn´t able to communicate with Freemaster at all (I got this error message: Can not detect the board information! The communication will be paused. Error code: 0x8000101 (Respose timout).)

If I use S32 with Freemaster KSDK I got the same issue doing the steps above. Can you guys send me an example build project using Freemaster, S9KEAZ128AVLH  and UART1?

Thanks in advance.

0 件の賞賛
返信

3,736件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please let me know what NXP part number used. Thanks.

0 件の賞賛
返信

3,736件の閲覧回数
diego_ambroggi
Contributor I

Hi Fang

I'm using S9KEAZ64AMLH

Best regards

Diego

0 件の賞賛
返信

3,736件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

It seems that your FreeMaster configuration is not correct. Please make reference from below post on step by step config the FreeMaster:

Tutorial: FreeMASTER Visualization and Run-Time Debugging | MCU on Eclipse 

0 件の賞賛
返信

3,695件の閲覧回数
sparkee
Contributor V

I know this is an old post but does it not seem ridiculous that an NXP employee recommends a third party blogger for information on how to use an NXP product?  

"How do you use our product?  There's a guy living in his mom's basement in Ottawa that figured it out, go ask him."

タグ(1)
0 件の賞賛
返信