Frdm-k64f

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Frdm-k64f

2,008 次查看
mukeshprasad
Contributor I

FRDM-k64F interface with SRDM -STBC -

AGMO1

Hi,

What are the setting requirement with Frdm-k64f board when interface with daughter board Frdm-STBC-AGMO1 when we are working with accelerometer and magnetometer sensor board mounted on FRDM-STBC-AGMO1.

0 项奖励
回复
2 回复数

1,733 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Please review the several kind of information about FRDM-STBC-AGM01.

FXAS21002C FXOS8700C 9-Axis Development Board|NXP

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,733 次查看
mukeshprasad
Contributor I

Hi,

What are software requirement for using this development board with frdm -k64f  board .

In this two board both have accelrometer and magnetometer sensor chip. how we  can differentiate while programming them individual.

For Eg : It for k64f board or STBC - AGMO1 board IC

Any setting in Tools or in hardware .while in writing code for sensor or program the board.

FRDM-k64f

FRDM-STBC-AGMO1

0 项奖励
回复