Frdm k64f prolonged output from pwm after disabling the timer input.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frdm k64f prolonged output from pwm after disabling the timer input.

953件の閲覧回数
Navkumar
Contributor I

Hi, 

I'm working on Frdm k64f kit. I've recently inherited a code base, which has hardware triggered ftm0 pwm, in turn driving two other pwms ftm1 and 2. However when the ftm0 timer is disabled there is a bit of residual data, value high for certain period from one of the pwm's. I have checked the settings and everything looks OK , being fairly new to this processor any help or nudge in the right direction is  much appreciated. Thanks. 

0 件の賞賛
返信
1 返信

941件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Navkumar,

Is there any documentation for the code base you got? Can you elaborate on how ftm0 is driving two other pwms ftm1 and 2? Otherwise, it is difficult to understand which phenomenon is correct, corresponding to the fact that you disable the ftm0 timer.

Maybe you can check the configuration of "40.4.10 Registers updated from write buffers" and "40.4.11 PWM synchronization" and "40.4.28 Global time base (GTB)" in K64P144M120SF5RM.

Best Regards,
Robin

0 件の賞賛
返信