Float and Double on K65

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Float and Double on K65

1,263件の閲覧回数
goranigic
Contributor II

I am using K65 in life science project. My customer insist to use double.

The built in single precision FPU + DSP will help or not?

Also, what is the impact on the processing speed?

Thank you,

0 件の賞賛
返信
1 返信

1,160件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Goran,

As you know that the K65 with FPU module can only do single precision float operation with hardware, and the DSP instructions in the Cortex-M4 only support integer or fixed point(fractional data) operation. Both the FPU and DSP instruction do not help to operate the double float operation.

Fortunately, the C compilers support double float operation by software simulation, but it takes a long time.

Hope it can help you.

BR

Xiangjun rong

0 件の賞賛
返信