Flexmemory as EEPROM in VLPR on K65F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexmemory as EEPROM in VLPR on K65F

958件の閲覧回数
jakub_tymejczyk
Contributor I

Hello,

Does EEPROM writes work in VLPR mode on K65F?

In AN11983 I found information that EEE writes are not allowed in VLPR and HSRUN modes, but that's different MCU.

I'm asking because it's not working in my case. Writing to EEPROM works before switching form RUN to VLPR mode and after switching from VLPR to RUN mode, but doesn't work in VLPR. Code execution does not crash when code tries to write to EEPROM but memory remains unchanged.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

862件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jakub Tymejczyk,

    K65F is the same, VLPR and HRUN mode, flash have limit function, please check this points in the K65F reference manual:

pastedImage_1.png

pastedImage_2.png

Wish it helps you!
Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信