Flexbus K63 controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbus K63 controller

1,476 Views
vinaysb
Contributor I

Hi All,

We are using  Flexbus to interface to an LCD. LCD is addressed using one bit Addr0. CS2 is used for LCD.

WE found that using logic analyzer. Addr0 is getting deasserted before the CS2 is getting asserted due to which LCD is not getting the Command.

Could some help us to identify the issue and fix the problem.

Thanks

Vinay S B

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,274 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Vinay,

please take a look on the Flexbus examples I attached to this post FlexBus in 16 bit mode and 8 bit access

They are usingK60 and K70 with CW and KDS. Some of the examples use TWR.LCD. They have also a document explaining the examples.

You may also take a look to AN4393

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply