Flexbus CS3 K63

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,828件の閲覧回数
aussiemate
Contributor II

I currently have an issue getting the Chip Select 3(CS3) Port C19 working with the flexbus on the K63 micro.

I already use CS0 and CS2 to access a PSRAM and LCD respectively.

I have setup the CS3 the same as the CS2 and I don't see the CS3 line change.

In the Manual it states that  CSCR[AA] bit must also be set, which I believe I have.

I have the following configuration.

PORTC->PCR[19] = PORT_PCR_MUX(5);                //CS_3

FB->CS[3].CSAR = 0x80000000

FB->CS[3].CSMR = FB_CSMR_V_MASK;   

FB->CS[3].CSCR = FB_CSCR_AA_MASK;

FB->CS[3].CSCR  |= (FB_CSCR_PS(2)|FB_CSCR_WS(0x0e));     

FB->CSPMCR = (FB_CSPMCR_GROUP4(1)|FB_CSPMCR_GROUP5(1));   

Has anyone else had issues getting the CS3 on flexbus working. 

Am I totally missing something?

Any Help greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,713件の閲覧回数
aussiemate
Contributor II

OK, My mistake the CS3 is working...  The settings mentioned above are ok.

Please don't ask why I thought it wasn't, it will only make me feel bad.  ( has to do with not actually monitoring the CS3 line)...

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,714件の閲覧回数
aussiemate
Contributor II

OK, My mistake the CS3 is working...  The settings mentioned above are ok.

Please don't ask why I thought it wasn't, it will only make me feel bad.  ( has to do with not actually monitoring the CS3 line)...

0 件の賞賛
返信