FlexNVM issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexNVM issue

1,570件の閲覧回数
Ming
Contributor III


I have three functions A, B, C. Both function A and B are mapped to FlexNVM sector (>= 0x1000000 in the memory map) and function C is allocated in the app flash sector. If I attempt to call function B from C, MCU got lost. I can see the disassembled code: instead of bl functionC to the correct address, the actual assmbly code is bogus: bl functionC_veneer (???? what's that?) which branches to an invalid address and causes an exception. My question is: is it possible to call a function located in FlexNVM region from normal flash region? If the caller is another function is the FlexNVM region, the jmp is correct.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,474件の閲覧回数
Ming
Contributor III

Let me be more specific here:

I am placing my boot loader code including Flash erase/write APIs generated by PE into FlexNVM region (>=0x1000000), separated from normal flash sect. I have a function called flash_entry(), in the map file, it's located at the following address:

.flash_operate
                0x100000dc       0xac ./Sources/flash_init_HW.o
                0x100000dc                a_reset
                0x10000120                flash_entry

Now from my app code, it attempts to enter boot loader mode by calling flash_entry(). Under debug mode, I can observe the disassembled branch instruction:

91        flash_entry();
0000f074:   bl __flash_entry_veneer (0x177b0); 0x000177b0

the assembly code branches address 0x177b0, which clearly is NOT the correction location. Please note that the instruction refers __flash_entry_veneer instead of flash_entry

If another function that is also located in the FlexNVM sector calls flash_entry(), it works expected.

65            flash_entry(); // never returns!
1000011a:   bl flash_entry (0x10000120); 0x10000120

Any suggestion what did I do wrong? Can caller from normal flash sector invoking function in the FlexNVM sector or vice versa?

0 件の賞賛
返信

1,474件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Ming Jiang,

I saw in our internal system that this problem is already solved. I will share the answer here in the community.

"If you place function B in FlexNVM section and invokes it from function A located in flash section, you can't single step into it at c level under debug mode, but it will branch to the correct function call after few steps."

Best regards,

Carlos

Technical Support Engineer

0 件の賞賛
返信