FlexCAN filter question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN filter question

1,649 Views
davidsherman
Senior Contributor I

I'm using the KE18F512, and I have the FlexCAN working in FIFO mode.  MCR[IDAM] = 0, CTRL2[RFFN] = 0, MCR[IRMQ]=1, CTRL2[EACEN] = 1, CTRL2[MRP] = 0.  The message buffers from 8-15 are being used for transmission only.  I am trying to filter standard frames, so I have the 8 FIFO filters set for 0x40000000, which should require the IDE bit.  However, both standard and extended frames are being received.  What am I doing wrong?

0 Kudos
Reply
2 Replies

1,384 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi David Sherman

Public information related with KE18F512 part number is not available yet, you need to contact your FAE to get support on this.

Sorry for the inconveniences that this may cause you.

Regards

Jorge Alcala

0 Kudos
Reply

1,384 Views
davidsherman
Senior Contributor I

The question was not about KE18, only about FlexCAN.  I got it figured out though.

0 Kudos
Reply