FlexCAN Mailboxes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,595件の閲覧回数
ivanrobles
Contributor III

How many mailboxes are there in FlexCAN?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,228件の閲覧回数
dereksnell
NXP Employee
NXP Employee

Hi Ivan,

It depends on the device, and how the FlexCAN peripheral is implemented.  You can find the specifics for the device in the Chip Configuration chapter of the Reference Manual.  Most Kinetis K devices have 16 message buffers per CAN peripheral.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,228件の閲覧回数
dereksnell
NXP Employee
NXP Employee

Hi Ivan,

It depends on the device, and how the FlexCAN peripheral is implemented.  You can find the specifics for the device in the Chip Configuration chapter of the Reference Manual.  Most Kinetis K devices have 16 message buffers per CAN peripheral.

0 件の賞賛
返信
2,228件の閲覧回数
sunilkonda
Contributor II

Hi Derek,

My application need to implement 32 message buffers, Is it possible to implement using RxFIFO. If possible, could you suggest me to how to implement that.

Thanks in advance.

Regards

Sunil

0 件の賞賛
返信