FlexCAN Interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN Interrupts

1,821件の閲覧回数
ivanrobles
Contributor III

Hi all.

I have a problem whit the interrupt Message buffer in FlexCAN.

I configured the interrupt as:

#define FLEXCAN_MB1_INT       1<<(37%32)

NVICICPR1 |= FLEXCAN_MB1_INT;
NVICISER1 |= FLEXCAN_MB1_INT;//Message buffer

then I set the flag in:

pFlexCANReg -> IMASK1 |= (1 << mailboxindex);  //for tansmit or receive

I use the Tower TWR-K60DN100M with other Microcontroller brand and I'm trying to comunnicate them.

When I transmit the message from the Tower to other device, it receives the message, the flag in IFLAG1 is setting,

but when I transmit from other device to TWR-K60DN100M, it doesn't receive the message , the Flag in IFLAG1 isn't setting. 

What's going on?

ラベル(1)
0 件の賞賛
返信
1 返信

1,459件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Ivan,

How did you initialize the flexCAN? Seems you are using FlexCAN1 for transmission, would you please give me details on the initial code? Thanks for your patience!!

B.R

Kan

0 件の賞賛
返信