FlexBus for Intel 8080 parallel bus transfers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexBus for Intel 8080 parallel bus transfers

2,196件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi everyone,

is somebody aware of an example code and circuit diagram that uses FlexBus (on K22) for emulating the Intel 8080 parallel bus implementation (separate Read and Write signals)?

Thanks a lot in advance.

Guenter

ラベル(2)
2 返答(返信)

1,573件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Guenter,

Please check the attachment.

The attachment is a FlexBus_LCD demo, the K22 control the LCD by using the Flexbus module.

2015-12-17_10-53-47.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,573件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi Ping,

thanks! This goes in the right direction. The speciality is that on Intel 8080 you have separate read and write signals (unlike on Motorola 6800 where a single R/W signal is used).

I don't know if anybody has ever worked on a solution with FlexBus to interface it to Intel 8080 bus with or without external logic.

br

Guenter

0 件の賞賛
返信