FlexBus_LCD presents

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexBus_LCD presents

FlexBus_LCD presents

This demo is about driving TFT LCD by FlexBus module on MAPS-K22 board.

      MAPS-K22 brief description:

  • High performance Freescale ARM Cortex™ M4 SoC MK22FN512VLL12​ with 120MHz core clock, 512KB Flash and 128K RAM.
  • Support Graphic LCD by Flexbus interface.
  • Power supply from Micro USB 5V.
  • Support ISO7816 smart card by UART interface.
  • Support connector for Peripheral, Application and Socket MAPS board.
  • SDK 1.0 Software release

Untitled.jpg

FlexBus Overview

      The FlexBus module is a hardware module that:

  • Provides memory expansion and provides connection to external peripherals with a parallel bus
  • Can be directly connected to the following asynchronous or synchronous slave-only devices with little or no additional circuitry:
  • External ROMs
  • Flash memories
  • Programmable logic devices
  • Other simple target (slave) devices

Block diagram

1.jpg

Pin functions

2015-09-11_16-07-44.jpg

Pins allocation

2015-09-11_16-10-15.jpg

Demo illustration

      After run the demo, the TFT LCD will display the Freescale logo as below, and I’ve also attached the demo.

Welcome to download it.

Untitled.jpg

标签 (1)
附件
无评分
版本历史
最后更新:
‎09-11-2015 01:22 AM
更新人: