Flashloader erased in FRDM-KV31F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashloader erased in FRDM-KV31F

1,293 Views
hyunkeenoh
Contributor II

HI, 

I have accidentally erased the preprogrammed Kinetis flashloader of MKV31F512 MCU in FRDM-KV31F.

How can I reprogram or download the flashloader into the MCU? Is it possible?

Thanks,

0 Kudos
Reply
1 Reply

1,144 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hyunkee Noh,

    Do you mean you erased the code which in the FRDM-KV31F which is out of factory? And you want to download it to the board again?

   If yes, please download the FRDM-KV31 QSP at first:

FRDM-KV31F Quick Start Package

Then you can find the pre-complied code in folder:

FRDM-KV31F-QSP\FRDM-KV31F_QSP\Pre-Compiled Demo Code

You can send the .bin file to your FRDM board device is ok.

 You also can refer to this link to get start:

FRDM-KV31F|Freedom Development Platform|Kinetis MCU|NXP 

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply