Flashing the user application - KW40/41

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing the user application - KW40/41

1,875 Views
sensenthuran
Contributor IV

Hi,

I am testing KW41 EVB.

I would like to flash an application (say, hci_app.bin) through UART connection.  I tried with blhost immediately after resetting the KW41W but  no response. 

I am using the default boot loader that came with.  Do we need to have any special boot loader?

Thanks

C:\FSL_Kinetis_Bootloader_1_2_0\FSL_Kinetis_Bootloader_1_2_0\bin\win>blhost.exe –d -p COM7,115200 -- get-property 1

[5a a6]

<>

<>

<>

Error: Initial ping failure: No response received for ping command.

Labels (1)
0 Kudos
Reply
2 Replies

1,523 Views
sensenthuran
Contributor IV

Thanks, I ll check with them.

0 Kudos
Reply

1,523 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I am assuming that you are a alpha customer, this information is not available.

Could you please contact your FAE or Sales Representative for more information.

Best Regards

Mario

0 Kudos
Reply