Flashing .elf file to S9KEAZ128AMLH

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing .elf file to S9KEAZ128AMLH

524 次查看
kaspt
Contributor II

I have a NXP MCU from the Kineties EA family S9KEAZ128AMLH https://www.nxp.com/part/S9KEAZ128AMLH. I want load .elf file to the flash and debug the target over SWD. I have a PEMicro universal adapter, MCU-Link, or St-Linkv2 which I can use.

Which software support flashing to NXP Kineties EA family?

Openocd does not support Kineties EA family. Does someone spend the effort to support the Kineties  EA family or has similar device?

There is PEMicro software PROGACMP for 200$. I don’t want to spend that amount for just flashing my device.

Alternative I There is PROGDSC for NXP DSC, but it seems that one does not support the target. Did I saw it right?

In a later step I want also debug the application. Preferably not depending on code-warrior or other windows only proprietary IDE.

Code warrior 11.1 has a problem when opening an empty workspace Error initializing Debug Database. See CW 11.1 Error - Error initializing Debug Database. - NXP Community

标记 (3)
0 项奖励
回复
1 回复

496 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @kaspt ,

Thank you for your post. I will answer your questions one by one.

1. Debugger: The KEA series MCU supports the PEMicro universal multilink. However, in the Supported Devices section of MCU Link JTAG/SWD Debug Probe | NXP Semiconductors, I didn't see that it supports the KEA series. The St-Link is not our product and should not be available.

2. Flash software Tool: You are correct that PROGDSC for NXP DSC does not support the KEA series.

3. IDE: According to Kinetis EA Sesries Family of Microcontrollers - One-Pager, the supported IDEs include CodeWarrior Elipse, S32DS for ARM, KDS, IAR, and Keil.

Celeste_Liu_0-1734321740927.png

I would recommend using CodeWarrior and S32DS for ARM more. They are free software from NXP that integrates programming, debugging and flashing functions. It can be used together with universal multilink of P&E.

S32DS for ARM: S32 Design Studio IDE for Arm® based MCUs | NXP Semiconductors

I understand that you have already downloaded CodeWarrior 11.1, so I recommend that you continue to use it. It can be confirmed that CW 11.1 can work properly on both Windows 10 and Windows 11. As for the problem of the error when creating a new empty workspace, let's see how to solve it together!

Hope it can help you.

Best Regards,

Celeste

0 项奖励
回复