Flashing MKW30Z over SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing MKW30Z over SWD

ソリューションへジャンプ
1,878件の閲覧回数
ivandrobyshevs1
Contributor II

I need to program MKW30Z via SWD, using another ARM chip's GPIO. It would be really helpful to see an example sequence for loading firmware to the chip, similar to the below code on github for EFM32. Is there  something like that in SDK, or may be in some open source project(s)?

PySWD/EFM32.py at master · disk91/PySWD · GitHub 

Thanks!

タグ(3)
0 件の賞賛
返信
1 解決策
1,732件の閲覧回数
ivandrobyshevs1
Contributor II

Turned out that recent OpenOCD supports KW30Z, and I was able to program it that way.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,733件の閲覧回数
ivandrobyshevs1
Contributor II

Turned out that recent OpenOCD supports KW30Z, and I was able to program it that way.

0 件の賞賛
返信