Flash read write example for MKE04Z8VTG4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash read write example for MKE04Z8VTG4

Jump to solution
4,993 Views
okaner
Contributor III

Hi,

       I am using MKE04Z microcontroller and SDK(SDK_2.9.0_MKE04Z8xxx4) . Is there any example how to use fsl_flash.c for this sdk. I saw pflash.c for the other microcontrollers but I think they use different sdk with different functions and parameters. Thank you.

Okan,

0 Kudos
Reply
1 Solution
4,980 Views
Anonymous
Deactivated User

hai okaner,

  I also having same issue but in the SDK Builder itself shows "The SDK does not include FRDM-KE04Z board project examples for MCUXpresso IDE" . So i refer MKE02 MCU for my reference and examples.

 

Thanks

Kalaimani Arumugam 

 

 

View solution in original post

0 Kudos
Reply
4 Replies
4,981 Views
Anonymous
Deactivated User

hai okaner,

  I also having same issue but in the SDK Builder itself shows "The SDK does not include FRDM-KE04Z board project examples for MCUXpresso IDE" . So i refer MKE02 MCU for my reference and examples.

 

Thanks

Kalaimani Arumugam 

 

 

0 Kudos
Reply
4,978 Views
okaner
Contributor III

Hi Kalaimani,

      I found examples for MKE02. Thank you very much. 

Okan,

0 Kudos
Reply
4,987 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi okaner,

  Can't you find the pflash demo from this link:

SDK_2.9.0_FRDM-KE04Z\boards\frdmke04z\driver_examples\flash\pflash

At lease, in the SDK 2.8.0, I still can find the pflash project, please check your SDK folder, whether you have that project or not?

If you still have issues about it, please kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply
4,984 Views
okaner
Contributor III

Hi Kerry,

     I have only uart example for both versions of SDK. In SDK Builder application, if I select filter for pflash.c example, in next step I cannot select Kinetis E series. 

Thanks,

a.png

0 Kudos
Reply