Flash procedure of the MKL02Z32VFM4 processor using Rx/Tx connection.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash procedure of the MKL02Z32VFM4 processor using Rx/Tx connection.

3,684 Views
edwardkäding
Contributor III

Hello Freescale Community,

I am new in this forum and appologise if this question has already been answered.

The customer support told me to write my questions in this forum so here I am.

I have finished programming the Freescale MKL02Z32VFM4 processor and also set up the Rx/Tx axynchronous serial communication with the main CPU (continous transfer and not Master / Slave).

In future we would like to be able to flash the KL02 MCU using the the main CPU.

Is it possible to flash the KL02-CPU using the same UART connection? Or do we need a second UART connection? Is it possible at all?

What is the flash procedure in general? Do we have to modify the internal programm when a flash command is set in motion or does it stop automatically etc..

Basically, all the information to implement a working flash procedure.

I thank everyone in advance who can help me.

Edward.

Labels (1)
0 Kudos
Reply
5 Replies

3,383 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Edward

Yes, you no need to use another UART channel.

The general process as below.

Main MCU send change flash command -> KL02 write a fixed byte a special value -> software reset -> enter bootloader mode -> program flash -> change that fixed byte to 0x00 -> software reset -> normal run mode -> UART communication.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply

3,383 Views
edwardkäding
Contributor III

Hi, Paul.

Thank you for your answer. I did not have the time to answer you recently.

Sadly it does not help me a noob like me at all. Therfore I have lots of open questions for (I apologise in advance!).

Main MCU send change flash command: - No problem there.

KL02 write a fixed byte a special value:

-     what is the "fixed byte"?

-     what is meant by special value and write it where?

Software Reset:

-     I have been trying to figure this out but do not know which register I have to write so the SYSRESETREQ is set ... ?

Enter Bootloader mode:

-     How can I enter this mode?

I am very sorry for all the questions, but I have to start from scratch.

Regards,

Edward.

0 Kudos
Reply

3,383 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Edward

Please see my comment below.

KL02 write a fixed byte a special value:

-     what is the "fixed byte"?

I think you can set to 0xAA

-     what is meant by special value and write it where?

One byte in flash where you do not place any code or other data.

Software Reset:

-     I have been trying to figure this out but do not know which register I have to write so the SYSRESETREQ is set ... ?

You can reference following code.

#define NVIC_SystemReset()   

{                                      

  SCB_AIRCR = SCB_AIRCR_VECTKEY(0x5FA)| SCB_AIRCR_SYSRESETREQ_MASK;     

  while(1);                                    

}

Enter Bootloader mode:

-     How can I enter this mode?

You can reference this application note. http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply

3,383 Views
edwardkäding
Contributor III

Hello Paul,

Thank you for your very quick response.

I hope I can take a look at your advices. I still have 3 other projects which I am working at.

Have a nice week,

Edward.

0 Kudos
Reply

3,383 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Edward

OK. No problem. Any questions, we can discuss in community.

Best Regards

Paul

0 Kudos
Reply