Flash driver C90TFS Partition MK10FX512VLQ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash driver C90TFS Partition MK10FX512VLQ12

3,637 Views
mrandreas
Contributor III

I'm using the C90TFS version Beta035 with the keil IDE on the MK10FX512VLQ12 target.

I'm able to init, erase block, erase sector,  verify block, verify section and FlashProgramPhrase.

But I'm not allowed to partition the flexmem. When I debug I get error code 0x4 = FTFx_ERR_ACCERR. Sometimes the unit restarts or crash in the FlashCommandSequence called from the DEFlashPartition.

It doesn't seem to be related to the EEEDataSizeCode or the DEPartitionCode. I'm not allowed to FlashEraseAllBlock blocks but I'm allowed to FlashEraseBlock so I loop through all blocks before doing the partition command.

Anny Ideas?

Labels (1)
0 Kudos
Reply
6 Replies

2,719 Views
mrandreas
Contributor III

Hi,

The following code is based on the asm from https://community.freescale.com/message/354833#354833

nDATA0          EQU     0x20

nDATA1          EQU     0x06

DATA0           EQU     nDATA0:AND:0x3F

DATA1           EQU     nDATA1:AND:0x0F

; </h>

                AREA    |.ARM.__AT_0x100003F8|, CODE, READONLY

                DCB     0xFF,  0xFF, 0xFF, 0xFF, DATA1, DATA0, 0xFF, 0xFF

                END

0x06 ends up in 0x100003FC and 0x20 in 0x100003FD this should be correct according to chapter 30.3.3 Data flash IFR map.

In the FlashInit command reads of FCCOBA register for EEEDataSetSize and FCCOBB register for DEPartitionCode. These registers are set to FF and not 0x06 and 0x20. This results in DFlash size 80000hx. Expected result is 40000 and 40000

Any Ideas?

0 Kudos
Reply

2,719 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the scatter file used in the application to program K70F512 Data Flash IFR:

; *************************************************************

; *** Scatter-Loading Description File generated by uVision ***

; *************************************************************

LR_IROM1 0x00000000 0x00080000  {    ; load region size_region

  ER_IROM1 0x00000000 0x00080000  {  ; load address = execution address

   .ANY (+RO)

  }

}

Check also, that flash algorithm  is flashing the IFR area.

Best Regards,

Luis

0 Kudos
Reply

2,719 Views
mrandreas
Contributor III

Her is the scatter file for my project:

LR_IROM1 0x00000000 0x00080000  {    ; load region size_region

  ER_IROM1 0x00000000 0x00080000  {  ; load address = execution address

   *.o (RESET, +First)

   *(InRoot$$Sections)

   .ANY (+RO)

  }

  RW_IRAM1 0x1FFF0000 0x00010000  {  ; RW data

   .ANY (+RW +ZI)

  }

}

If I have understood "flashing the IFR area correct"; As mention in the previous post the asm code sets 0x06 in 0x100003FC and 0x20 in 0x100003FD. This is verified by running the asm from one project and reading the memory assignment from another. Is the IFR address correct (0x100003FC & 0x100003FD)?

0 Kudos
Reply

2,719 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

As I told you, this is for K70FX512 and the code project was coming from Keil and verified at least, for a customer. You will have to review it in your own derivative. Or contact Keil to ask for the right configturation of your derivative. Using Pemicro you can flash the locations in the connection settings (also with Keil) , with ulink you need to go in this way, running the code to flash the locations.

Luis

0 Kudos
Reply

2,719 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Please, check my answer to this threat in case that can also help you.

https://community.freescale.com/message/354833#354833

Luis

0 Kudos
Reply

2,719 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello mrandreas,

Please have a look at this Application note from Keil, and also at the Reference Manual of your device.

http://www.keil.com/appnotes/files/apnt220.pdf

Regards!

0 Kudos
Reply