Flash Loader Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash Loader Error

1,876 次查看
niket_zope
Contributor III

I am working on mke15z256vll7 nxp kinectics controller.

I made some modification in linker script for my project.

But unable to flash the code.

I tried flashing sdk led_blinky same issue !!!

What went worng ? How to over come this ? @kerryzhou @nxf56274 

Fri Aug 20, 2021 11:20:41: IAR Embedded Workbench 8.42.2 (C:\software\IAR\arm\bin\armproc.dll)
Fri Aug 20, 2021 11:20:41: Loaded macro file: C:\software\IAR\arm\config\debugger\NXP\KE1xF.dmac
Fri Aug 20, 2021 11:20:41: Loaded macro file: C:\software\IAR\arm\config\flashloader\NXP\FlashKE1xZ7.mac
Fri Aug 20, 2021 11:20:41: JLINK command: ProjectFile = C:\Users\niket.zope\Downloads\SDK_2.8.0_FRDM-KE15Z\boards\frdmke15z\demo_apps\led_blinky\iar\settings\led_blinky_debug.jlink, return = 0
Fri Aug 20, 2021 11:20:41: Device "MKE15Z256XXX7" selected.
Fri Aug 20, 2021 11:20:41: DLL version: V6.94 , compiled Jan 8 2021 13:01:30
Fri Aug 20, 2021 11:20:41: Firmware: J-Link OpenSDA 2 compiled Oct 10 2018 16:29:51
Fri Aug 20, 2021 11:20:41: Selecting SWD as current target interface.
Fri Aug 20, 2021 11:20:41: JTAG speed is initially set to: 32 kHz
Fri Aug 20, 2021 11:20:41: InitTarget() start
Fri Aug 20, 2021 11:20:41: InitTarget()
Fri Aug 20, 2021 11:20:41: Connect Under Reset
Fri Aug 20, 2021 11:20:42: Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.
Fri Aug 20, 2021 11:20:42: For debugger connection the device needs to be unsecured.
Fri Aug 20, 2021 11:20:42: Note: Unsecuring will trigger a mass erase of the internal flash.
Fri Aug 20, 2021 11:20:42: Executing default behavior previously saved in the registry.
Fri Aug 20, 2021 11:20:42: Device will be unsecured now.
Fri Aug 20, 2021 11:20:42: InitTarget() end
Fri Aug 20, 2021 11:20:42: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:42: DPv0 detected
Fri Aug 20, 2021 11:20:42: Scanning AP map to find all available APs
Fri Aug 20, 2021 11:20:42: AP[2]: Stopped AP scan as end of AP map has been reached
Fri Aug 20, 2021 11:20:42: AP[0]: AHB-AP (IDR: 0x04770031)
Fri Aug 20, 2021 11:20:42: AP[1]: JTAG-AP (IDR: 0x001C0020)
Fri Aug 20, 2021 11:20:42: Iterating through AP map to find AHB-AP to use
Fri Aug 20, 2021 11:20:42: AP[0]: Core found
Fri Aug 20, 2021 11:20:42: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:42: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:42: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:42: FPUnit: 2 code (BP) slots and 0 literal slots
Fri Aug 20, 2021 11:20:42: CoreSight components:
Fri Aug 20, 2021 11:20:42: ROMTbl[0] @ F0002000
Fri Aug 20, 2021 11:20:42: ROMTbl[0][0]: F0000000, CID: B105900D, PID: 001BB932 MTB-M0+
Fri Aug 20, 2021 11:20:42: ROMTbl[0][2]: E00FF000, CID: B105100D, PID: 000BB4C0 ROM Table
Fri Aug 20, 2021 11:20:42: ROMTbl[1] @ E00FF000
Fri Aug 20, 2021 11:20:42: ROMTbl[1][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
Fri Aug 20, 2021 11:20:42: ROMTbl[1][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
Fri Aug 20, 2021 11:20:42: ROMTbl[1][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
Fri Aug 20, 2021 11:20:42: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:42: Reset: Reset device via AIRCR.SYSRESETREQ.
Fri Aug 20, 2021 11:20:42: Reset: S_RESET_ST never gets cleared. CPU seems to be kept in reset forever.
Fri Aug 20, 2021 11:20:42: Reset: Using fallback: Reset pin.
Fri Aug 20, 2021 11:20:42: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:42: Reset: Reset device via reset pin
Fri Aug 20, 2021 11:20:43: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Aug 20, 2021 11:20:43: Reset: Reconnecting and manually halting CPU.
Fri Aug 20, 2021 11:20:43: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:43: DPv0 detected
Fri Aug 20, 2021 11:20:43: AP map detection skipped. Manually configured AP map found.
Fri Aug 20, 2021 11:20:43: AP[0]: AHB-AP (IDR: Not set)
Fri Aug 20, 2021 11:20:43: AP[0]: Core found
Fri Aug 20, 2021 11:20:43: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:43: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:43: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:43: CPU could not be halted
Fri Aug 20, 2021 11:20:43: Reset: Core did not halt after reset, trying to disable WDT.
Fri Aug 20, 2021 11:20:43: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:43: Reset: Reset device via reset pin
Fri Aug 20, 2021 11:20:43: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Aug 20, 2021 11:20:43: Reset: Reconnecting and manually halting CPU.
Fri Aug 20, 2021 11:20:43: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:43: DPv0 detected
Fri Aug 20, 2021 11:20:43: AP map detection skipped. Manually configured AP map found.
Fri Aug 20, 2021 11:20:43: AP[0]: AHB-AP (IDR: Not set)
Fri Aug 20, 2021 11:20:43: AP[0]: Core found
Fri Aug 20, 2021 11:20:43: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:43: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:43: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:44: CPU could not be halted
Fri Aug 20, 2021 11:20:44: Reset: Failed. Toggling reset pin and trying reset strategy again.
Fri Aug 20, 2021 11:20:44: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:44: DPv0 detected
Fri Aug 20, 2021 11:20:44: AP map detection skipped. Manually configured AP map found.
Fri Aug 20, 2021 11:20:44: AP[0]: AHB-AP (IDR: Not set)
Fri Aug 20, 2021 11:20:44: AP[0]: Core found
Fri Aug 20, 2021 11:20:44: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:44: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:44: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:44: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:44: Reset: Reset device via AIRCR.SYSRESETREQ.
Fri Aug 20, 2021 11:20:44: Reset: S_RESET_ST never gets cleared. CPU seems to be kept in reset forever.
Fri Aug 20, 2021 11:20:44: Reset: Using fallback: Reset pin.
Fri Aug 20, 2021 11:20:44: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:44: Reset: Reset device via reset pin
Fri Aug 20, 2021 11:20:44: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Aug 20, 2021 11:20:44: Reset: Reconnecting and manually halting CPU.
Fri Aug 20, 2021 11:20:44: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:44: DPv0 detected
Fri Aug 20, 2021 11:20:44: AP map detection skipped. Manually configured AP map found.
Fri Aug 20, 2021 11:20:44: AP[0]: AHB-AP (IDR: Not set)
Fri Aug 20, 2021 11:20:45: AP[0]: Core found
Fri Aug 20, 2021 11:20:45: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:45: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:45: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:45: CPU could not be halted
Fri Aug 20, 2021 11:20:45: Reset: Core did not halt after reset, trying to disable WDT.
Fri Aug 20, 2021 11:20:45: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Aug 20, 2021 11:20:45: Reset: Reset device via reset pin
Fri Aug 20, 2021 11:20:45: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Aug 20, 2021 11:20:45: Reset: Reconnecting and manually halting CPU.
Fri Aug 20, 2021 11:20:45: Found SW-DP with ID 0x0BC11477
Fri Aug 20, 2021 11:20:45: DPv0 detected
Fri Aug 20, 2021 11:20:45: AP map detection skipped. Manually configured AP map found.
Fri Aug 20, 2021 11:20:45: AP[0]: AHB-AP (IDR: Not set)
Fri Aug 20, 2021 11:20:45: AP[0]: Core found
Fri Aug 20, 2021 11:20:45: AP[0]: AHB-AP ROM base: 0xF0002000
Fri Aug 20, 2021 11:20:45: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Fri Aug 20, 2021 11:20:45: Found Cortex-M0 r0p1, Little endian.
Fri Aug 20, 2021 11:20:45: CPU could not be halted
Fri Aug 20, 2021 11:20:45: AfterResetTarget() start
Fri Aug 20, 2021 11:20:45: AfterResetTarget()
Fri Aug 20, 2021 11:20:45: AfterResetTarget() end
Fri Aug 20, 2021 11:20:45: CPU could not be halted
Fri Aug 20, 2021 11:20:45: Warning: Failed to halt CPU.
Fri Aug 20, 2021 11:20:45: Hardware reset with strategy 0 was performed
Fri Aug 20, 2021 11:20:45: Initial reset was performed
Fri Aug 20, 2021 11:20:46: CPU could not be halted
Fri Aug 20, 2021 11:20:47: DMAC: Disable watchdog ...
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 2 (R2) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 3 (R3) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 4 (R4) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 5 (R5) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 6 (R6) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 7 (R7) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 8 (R8) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 9 (R9) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 10 (R10) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 11 (R11) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 12 (R12) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 17 (MSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 18 (PSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 14 (R14) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 16 (XPSR) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 20 (CFBP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 2 (R2) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 3 (R3) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 4 (R4) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 5 (R5) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 6 (R6) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 7 (R7) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 8 (R8) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 9 (R9) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 10 (R10) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 11 (R11) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 12 (R12) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 17 (MSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 18 (PSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 14 (R14) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 16 (XPSR) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 20 (CFBP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 2 (R2) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 3 (R3) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 4 (R4) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 5 (R5) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 6 (R6) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 7 (R7) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 8 (R8) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 9 (R9) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 10 (R10) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 11 (R11) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 12 (R12) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 17 (MSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 18 (PSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 14 (R14) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 16 (XPSR) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 20 (CFBP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: CPU is not halted
Fri Aug 20, 2021 11:20:47: CPU could not be halted
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 2 (R2) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 3 (R3) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 4 (R4) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 5 (R5) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 6 (R6) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 7 (R7) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 8 (R8) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 9 (R9) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 10 (R10) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 11 (R11) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 12 (R12) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 17 (MSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 18 (PSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 14 (R14) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 16 (XPSR) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 20 (CFBP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 0 (R0) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 1 (R1) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 2 (R2) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 3 (R3) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 4 (R4) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 5 (R5) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 6 (R6) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 7 (R7) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 8 (R8) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 9 (R9) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 10 (R10) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 11 (R11) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 12 (R12) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 17 (MSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 18 (PSP) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 14 (R14) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 15 (R15) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 16 (XPSR) while CPU is running
Fri Aug 20, 2021 11:20:47: Warning: Cannot read register 20 (CFBP) while CPU is running
Fri Aug 20, 2021 11:20:47: ----- Prepare hardware for Flashloader -----
Fri Aug 20, 2021 11:20:47: 1784 bytes downloaded and verified (3.71 Kbytes/sec)
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF000, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF001, target byte: 0xAA, byte in file: 0x30
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF002, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF003, target byte: 0xAA, byte in file: 0x20
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF004, target byte: 0xF9, byte in file: 0xFD
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF005, target byte: 0xF1, byte in file: 0xF4
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF008, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF009, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF00A, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF00B, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF021, target byte: 0xF9, byte in file: 0xB5
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF022, target byte: 0xFF, byte in file: 0x1C
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF023, target byte: 0x1C, byte in file: 0x4C
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF024, target byte: 0xAA, byte in file: 0x20
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF025, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF026, target byte: 0xAA, byte in file: 0x18
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF027, target byte: 0xAA, byte in file: 0x30
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF058, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF059, target byte: 0xAA, byte in file: 0x29
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF05A, target byte: 0xAA, byte in file: 0x0D
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF05B, target byte: 0xAA, byte in file: 0xD1
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF14C, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF14D, target byte: 0xAA, byte in file: 0x24
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF14E, target byte: 0xAA, byte in file: 0x45
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF14F, target byte: 0xAA, byte in file: 0x18
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF15C, target byte: 0xAA, byte in file: 0x08
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF15D, target byte: 0xAA, byte in file: 0x35
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF15E, target byte: 0xAA, byte in file: 0x08
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF15F, target byte: 0xAA, byte in file: 0x36
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF19C, target byte: 0xAA, byte in file: 0x40
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF19D, target byte: 0xAA, byte in file: 0x78
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF19E, target byte: 0xAA, byte in file: 0x60
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF19F, target byte: 0xAA, byte in file: 0x70
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1B0, target byte: 0xAA, byte in file: 0x88
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1B1, target byte: 0xAA, byte in file: 0x42
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1B2, target byte: 0xAA, byte in file: 0x1B
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1B3, target byte: 0xAA, byte in file: 0xD2
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1D5, target byte: 0x73, byte in file: 0x71
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF1D7, target byte: 0x70, byte in file: 0x72
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF288, target byte: 0xAA, byte in file: 0x03
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF289, target byte: 0xAA, byte in file: 0xD1
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF28A, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF28B, target byte: 0xAA, byte in file: 0x2B
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF554, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF555, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF556, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF557, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF578, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF579, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF57A, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:47: Warning:
Fri Aug 20, 2021 11:20:47: Verify error at address 0x1FFFF57B, target byte: 0xAA, byte in file: 0x00
Fri Aug 20, 2021 11:20:53: Fatal error: There were warnings during download of FLASH loader, see Log Window Session aborted!
Fri Aug 20, 2021 11:20:53: Failed to load flash loader: C:\software\IAR\arm\config\flashloader\NXP\FlashKE1xZ7RAM16K.out
Fri Aug 20, 2021 11:20:53: Unloaded macro file: C:\software\IAR\arm\config\flashloader\NXP\FlashKE1xZ7.mac
Fri Aug 20, 2021 11:20:53: IAR Embedded Workbench 8.42.2 (C:\software\IAR\arm\bin\armproc.dll)

0 项奖励
回复
1 回复

1,863 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @niket_zope 

Do you use the FRDM-KE15Z board? This board can download the SDK code directly.

What's the SDK version you are using? You need to use the newest SDK 2.10.0:

https://mcuxpresso.nxp.com/

In this version, the IAR version should be:IAR Embedded Workbench for ARM, version is 9.10.2

Your IAR 8.x is old, you need to update your IAR and SDK version, then try it again.

If you still meet issues, just kindly let me know.

Best Regards,

kerry

0 项奖励
回复