Flash Driver for KEA-128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Driver for KEA-128

2,806件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

I want a example Flash Driver for KEA-128. My aim is to store some data in Flash and change it at run time in Flash and on next bootup I want the changed values to reflect in the code while bootup or after start itself.Please provide me this example with documents and example code :smileyhappy:

ラベル(2)
2 返答(返信)

2,426件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

After had a brief look through the statement above, I'd highly recommend you to use the EEPROM Emulation Driver to achieve data storage of application variables that must be maintained when power is removed and need to be updated individually during run-time.

You can download the EEPROM emulation driver for KEA128 through the link as below.

KEA Reliable, Low-power MCUs|NXP

2016-05-23_15-01-01.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,426件の閲覧回数
mortyhsueh
Contributor II

Hi,

I think this official EEE (EEPROM emulation) driver for KEA128 can help you.

http://cache.nxp.com/files/32bit/software_tools/KEAZN8_64_EEE_DEVD.exe

0 件の賞賛
返信