Flash Config section

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,464件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I have an ugly issue with the compiler.

I want to define the configuration words in the source code. That's what I do

static __attribute__ ((section (".FlashConfig"))) const cfm_t _cfm =
{
.backkey[ 0 ] = 0x01,
.backkey[ 1 ] = 0x02,
.backkey[ 2 ] = 0x03,

......

The fields are expanded..

If in the startup file .s I use the original declaration

.section .FlashConfig, "a"
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFF7DFE

The linking process advices the FlashConfig section is too small to guest both data .That's what I expect.

Bit if I comment the assembly declaration, the C declared data _cfm  disappears. Simply it does not exist in the map file.

I don't find a reason why.

Suggestions??

Thank You

Pietro

タグ(1)
1 解決策
6,663件の閲覧回数
mjbcswitzerland
Specialist V

Hi Pietro

For GCC:

const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
    KINETIS_FLASH_CONFIGURATION_BACKDOOR_KEY,
    KINETIS_FLASH_CONFIGURATION_PROGRAM_PROTECTION,
    KINETIS_FLASH_CONFIGURATION_SECURITY,
    KINETIS_FLASH_CONFIGURATION_NONVOL_OPTION,
    KINETIS_FLASH_CONFIGURATION_EEPROM_PROT,
    KINETIS_FLASH_CONFIGURATION_DATAFLASH_PROT
};

In linker script

  .f_config ALIGN(__Fconfig_segment_start__ , 4) :
  {
    __flash_config = .;
    KEEP(*(.f_config .f_config.*))
  }

You NEED the KEEP so that the linker doesn't optimise the data away since it doesn't find it being accessed by any code.

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
6,663件の閲覧回数
pietrodicastri
Senior Contributor II

Hei Mark

The implementation gives the result to have the structure in the map file.

Like this

.FlashConfig 0x00000400 0x10
0x00000400 . = ALIGN (0x4)
0x00000400 _cfm = .
*(.FlashConfig .FlashConfig.*)
.FlashConfig 0x00000400 0x10 ./Sources/chip_cfg.o
0x00000410 . = ALIGN (0x4)

But when I try to program the memory dump of the address 0x400 is not reflecting the content of the _cfm..

What can it be?

Thank  You

Pietro

0 件の賞賛
返信
6,663件の閲覧回数
mjbcswitzerland
Specialist V

Hi Pietro

If you see the sector in the map file I would expect it to be in your binary too.

Look at the binary file (or srec) content with a binary editor - maybe it is there but being filled with unexpected data - such as 0xff (?).

Regards

Mark

 


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

6,663件の閲覧回数
pietrodicastri
Senior Contributor II

Hei Mark

Thank You for following. Now I have the data in the flash. I have another problem in the bit field interpretation.

But for now I can live with what I have, I need to concentrate on another issue.

I created another thread, Flash writes with breakpoints NOT without. If You can give a look it would be helpful.

Thank You

Pietro

0 件の賞賛
返信
6,663件の閲覧回数
mjbcswitzerland
Specialist V

Hello Pietro

These may help with some field interpretations.

typedef struct _PACK stKINETIS_FLASH_CONFIGURATION    // loaded from FLASH 0x00000400 at reset
{
    unsigned char  ucBackdoorComparisonKey[8];
    unsigned long  ulProgramFlashProtection;
    unsigned char  ucFlashSecurity;
    unsigned char  ucNonvolatileOption;
    unsigned char  ucEEPROM_protection;
    unsigned char  ucDataFlashProtection;
} KINETIS_FLASH_CONFIGURATION;

const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
    {BACKDOOR_KEY_0, BACKDOOR_KEY_1, BACKDOOR_KEY_2, BACKDOOR_KEY_3, BACKDOOR_KEY_4, BACKDOOR_KEY_5, BACKDOOR_KEY_6, BACKDOOR_KEY_7},
    (0xffffffff),       // PROT[31:24]:PROT[23:16]:PROT[15:8]:PROT[7:0] - no protection when all are '1'
    KINETIS_FLASH_CONFIGURATION_SECURITY,
    KINETIS_FLASH_CONFIGURATION_NONVOL_OPTION,
    KINETIS_FLASH_CONFIGURATION_EEPROM_PROT,
    KINETIS_FLASH_CONFIGURATION_DATAFLASH_PROT
};


Regards

Mark

 


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

6,663件の閲覧回数
pietrodicastri
Senior Contributor II

Thank You

I will enjoy this suggestion when the bootloader will work. Now the crashing of the flash writing is booking me fully.

Thank You

Pietro

0 件の賞賛
返信
6,664件の閲覧回数
mjbcswitzerland
Specialist V

Hi Pietro

For GCC:

const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
    KINETIS_FLASH_CONFIGURATION_BACKDOOR_KEY,
    KINETIS_FLASH_CONFIGURATION_PROGRAM_PROTECTION,
    KINETIS_FLASH_CONFIGURATION_SECURITY,
    KINETIS_FLASH_CONFIGURATION_NONVOL_OPTION,
    KINETIS_FLASH_CONFIGURATION_EEPROM_PROT,
    KINETIS_FLASH_CONFIGURATION_DATAFLASH_PROT
};

In linker script

  .f_config ALIGN(__Fconfig_segment_start__ , 4) :
  {
    __flash_config = .;
    KEEP(*(.f_config .f_config.*))
  }

You NEED the KEEP so that the linker doesn't optimise the data away since it doesn't find it being accessed by any code.

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 件の賞賛
返信