Flash Access Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash Access Error

跳至解决方案
4,249 次查看
renka
Contributor II

I'am currently working with K26f processor with KDS3.2 and KSDSK v1.3. Core clock is 180Mhz,Flash Clock is 25.71 Mhz as Processor Expert recommends...

I imported Flash Driver component into my project,selected the address to erase in internal flash,but FlashErase () returns me error 0x20 - Flash Access Memory.Following is my code after importing "Flash Driver Component" from Component Library.

#define LAUNCH_CMD_SIZE 0x100
pFLASHCOMMANDSEQUENCE g_FlashLaunchCommand = (pFLASHCOMMANDSEQUENCE)0xFFFFFFFF;
// Array to copy __Launch_Command func to RAM.
uint16_t ramFunc[LAUNCH_CMD_SIZE/2];

uint32_t destAdrss = (uint32_t *)0x0001efff ;
// Set command to RAM.
g_FlashLaunchCommand = (pFLASHCOMMANDSEQUENCE)RelocateFunction((uint32_t)ramFunc , LAUNCH_CMD_SIZE ,(uint32_t)FlashCommandSequence);
INT_SYS_DisableIRQGlobal();
uint32_t result = FlashEraseSector(&flash1_InitConfig0,destAdrss,FSL_FEATURE_FLASH_PFLASH_BLOCK_SECTOR_SIZE,
g_FlashLaunchCommand);
INT_SYS_EnableIRQGlobal();

result backs to me error 0x20 - Flash Access Error....

What's wrong here?

Thanks in advance.

1 解答
3,850 次查看
mjbcswitzerland
Specialist V

Hi

pastedImage_1.png

This will explain if you are in HSRUN mode. To program flash you need to be in RUN mode (max. 120Mhz CPU clock).

Regards

Mark

在原帖中查看解决方案

4 回复数
3,850 次查看
renka
Contributor II

Thank you very much. It's working.

0 项奖励
回复
3,851 次查看
mjbcswitzerland
Specialist V

Hi

pastedImage_1.png

This will explain if you are in HSRUN mode. To program flash you need to be in RUN mode (max. 120Mhz CPU clock).

Regards

Mark

2,996 次查看
fitz-nguyen
Contributor I

The solution work !!! 

this help me alot. Thank for very helpful advise. 

Regards.

0 项奖励
回复
3,850 次查看
abdullahkahrama
Contributor IV

I was having kStatus_FLASH_AccessError while using FLASH_Erase command with Kinetis SDK 2.2 with a K02F microcontroller.

I was puzzled why it had such an issue until I saw your answer. Thank you very much. I really appreciate your this and other countless helps to the community.

0 项奖励
回复