Fault input disable FTM output for KV11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fault input disable FTM output for KV11

Jump to solution
1,100 Views
admin
Specialist II

Original Content posted by Li Yang 

For KV11, the fault input is used for disable PWM output, could you help answer the following two questions?

1. If FTM0_FLT0 is enabled, all channels of FTM0 output are disabled or only FTM0_CH0/FTM0_CH1 are disabled?

2. Whether FTM1_FLT0 can be used to disable PWM output of FTM0_CH0/FTM0_CH1?

Thanks!

note:

The customer name is Suzhou Norlha, the project is electric wheelchair. 

Labels (1)
0 Kudos
Reply
1 Solution
918 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Li Yang,

According to the reference manual, there are two group of bits for configuring the fault control feature of channels.

The FAULTM[1:0] is used to configure the general fault control mode, and the FAULTENn bit is used to enable or disable the fault control feature of the specific pair of the channels.

So it's available to enable one pair of channels in the FTM module.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
919 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Li Yang,

According to the reference manual, there are two group of bits for configuring the fault control feature of channels.

The FAULTM[1:0] is used to configure the general fault control mode, and the FAULTENn bit is used to enable or disable the fault control feature of the specific pair of the channels.

So it's available to enable one pair of channels in the FTM module.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply