Fault input disable FTM output for KV11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fault input disable FTM output for KV11

ソリューションへジャンプ
1,612件の閲覧回数
admin
Specialist II

Original Content posted by Li Yang 

For KV11, the fault input is used for disable PWM output, could you help answer the following two questions?

1. If FTM0_FLT0 is enabled, all channels of FTM0 output are disabled or only FTM0_CH0/FTM0_CH1 are disabled?

2. Whether FTM1_FLT0 can be used to disable PWM output of FTM0_CH0/FTM0_CH1?

Thanks!

note:

The customer name is Suzhou Norlha, the project is electric wheelchair. 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,430件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Li Yang,

According to the reference manual, there are two group of bits for configuring the fault control feature of channels.

The FAULTM[1:0] is used to configure the general fault control mode, and the FAULTENn bit is used to enable or disable the fault control feature of the specific pair of the channels.

So it's available to enable one pair of channels in the FTM module.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,431件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Li Yang,

According to the reference manual, there are two group of bits for configuring the fault control feature of channels.

The FAULTM[1:0] is used to configure the general fault control mode, and the FAULTENn bit is used to enable or disable the fault control feature of the specific pair of the channels.

So it's available to enable one pair of channels in the FTM module.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信