Fatal warning used IAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fatal warning used IAR

2,751 Views
zhaoqinsu
NXP Employee
NXP Employee

Who know the reason of in the picture just when I debug used IAR7.4?

Thank you very much!Untitled.png

0 Kudos
Reply
2 Replies

2,667 Views
mjbcswitzerland
Specialist V

Hi

99% percent sure that it is because you haven't programmed any code to the processor.

Make sure that you don't have the debugger set up to not download code - use download and connect, and not just connect.

Regards

Mark

0 Kudos
Reply

2,667 Views
zhaoqinsu
NXP Employee
NXP Employee

Yes ,that is focus  what I have  to ask . I had download and connected to device , but why it can not  to download in or debug ?

0 Kudos
Reply