FTM Multi-channel capture of pwm input will cause code unstable?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM Multi-channel capture of pwm input will cause code unstable?

5,321 Views
erichsu
Contributor I

FTM0 channel pair 0 uses channels 0 and 1, channel pair 1 uses channels 2 and 3, but  capture of pwm input will cause program instability. Is the way to enable and disable interrupts incorrect?

erichsu_0-1619092967531.png

 

0 Kudos
Reply
5 Replies

5,282 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Eric,

Could you please let us know what is the part number you are using?

Best regards,

Felipe

0 Kudos
Reply

5,273 Views
erichsu
Contributor I

FRDM-KV11Z

pin configuration:

erichsu_0-1619538131077.png

 

0 Kudos
Reply

5,260 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Eric,

Thank you for your reply. I see you are using ftm_dual_edge_capture example from the SDK as a starting point. Is there an issue if you run example code with no modifications? Could you please provide what did you modify in the example? This will help us narrow down where the issue could be.

Additionally, could you please let me know what specific line of your code is the MCU halting?

Best regards,

Felipe

0 Kudos
Reply

5,242 Views
erichsu
Contributor I

I see you are using ftm_dual_edge_capture example from the SDK as a starting point. Is there an issue if you run example code with no modifications? 

Ans: no problem

Could you please provide what did you modify in the example?

Ans: Modify in the exapmle

erichsu_0-1619964913036.png

erichsu_1-1619964946292.png

while(1)
{
// while (ftmFirstChannelInterruptFlag_PITCH != true)
//{
//}

// while (ftmSecondChannelInterruptFlag_PITCH != true)
// {
// }
#if 1
if ((ftmFirstChannelInterruptFlag_PITCH == true) && (ftmSecondChannelInterruptFlag_PITCH == true))
{
ftmFirstChannelInterruptFlag_PITCH = false;
ftmSecondChannelInterruptFlag_PITCH = false;

/* Clear first channel interrupt flag after the second edge is detected.*/
FTM_ClearStatusFlags(DEMO_FTM_BASEADDR, FTM_FIRST_CHANNEL_PITCH_FLAG);

/* Clear overflow interrupt flag.*/
FTM_ClearStatusFlags(DEMO_FTM_BASEADDR, kFTM_TimeOverflowFlag);
/* Disable overflow interrupt.*/
FTM_DisableInterrupts(DEMO_FTM_BASEADDR, kFTM_TimeOverflowInterruptEnable);

capture1Val_pitch = DEMO_FTM_BASEADDR->CONTROLS[BOARD_FTM_INPUT_CAPTURE_CHANNEL_PAIR_PITCH * 2].CnV;
capture2Val_pitch = DEMO_FTM_BASEADDR->CONTROLS[(BOARD_FTM_INPUT_CAPTURE_CHANNEL_PAIR_PITCH * 2) + 1].CnV;


/* FTM clock source is not prescaled and is
* divided by 1000000 as the output is printed in microseconds
*/
if(capture2Val_pitch > capture1Val_pitch)
{
//PRINTF("\r\nCapture value PITCH C(n)V=%x\r\n", capture1Val_pitch);
//PRINTF("\r\nCapture value PITCH C(n+1)V=%x\r\n", capture2Val_pitch);
pulseWidth_pitch =
(float)(((g_secondChannelOverflowCount_PITCH - g_firstChannelOverflowCount_PITCH) * 65536 + capture2Val_pitch - capture1Val_pitch) +
1) /
((float)FTM_SOURCE_CLOCK / 1000000);
//PRINTF("\r\nInput signals frequency = %f hz\r\n", 1/(pulseWidth_pitch*2)*1000000);
PRINTF("\r\nInput signals PITCH pulse width = %f us\r\n", pulseWidth_pitch);
}
g_secondChannelOverflowCount_PITCH = 0;
g_firstChannelOverflowCount_PITCH = 0;

/* Enable first channel interrupt */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, FTM_FIRST_CHANNEL_INTERRUPT_ENABLE_PITCH);

/* Enable second channel interrupt when the second edge is detected */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, FTM_SECOND_CHANNEL_INTERRUPT_ENABLE_PITCH);

/* Enable overflow interrupt */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, kFTM_TimeOverflowInterruptEnable);
}
#endif
if ((ftmFirstChannelInterruptFlag_YAW == true) && (ftmSecondChannelInterruptFlag_YAW == true))
{
ftmFirstChannelInterruptFlag_YAW = false;
ftmSecondChannelInterruptFlag_YAW = false;

/* Clear first channel interrupt flag after the second edge is detected.*/
FTM_ClearStatusFlags(DEMO_FTM_BASEADDR, FTM_FIRST_CHANNEL_YAW_FLAG);

/* Clear overflow interrupt flag.*/
FTM_ClearStatusFlags(DEMO_FTM_BASEADDR, kFTM_TimeOverflowFlag);
/* Disable overflow interrupt.*/
FTM_DisableInterrupts(DEMO_FTM_BASEADDR, kFTM_TimeOverflowInterruptEnable);

capture1Val_yaw = DEMO_FTM_BASEADDR->CONTROLS[BOARD_FTM_INPUT_CAPTURE_CHANNEL_PAIR_YAW * 2].CnV;
capture2Val_yaw = DEMO_FTM_BASEADDR->CONTROLS[(BOARD_FTM_INPUT_CAPTURE_CHANNEL_PAIR_YAW * 2) + 1].CnV;


/* FTM clock source is not prescaled and is
* divided by 1000000 as the output is printed in microseconds
*/
if(capture2Val_yaw > capture1Val_yaw)
{
//PRINTF("\r\nCapture value YAW C(n)V=%x\r\n", capture1Val_yaw);
//PRINTF("\r\nCapture value YAW C(n+1)V=%x\r\n", capture2Val_yaw);
pulseWidth_yaw =
(float)(((g_secondChannelOverflowCount_YAW - g_firstChannelOverflowCount_YAW) * 65536 + capture2Val_yaw - capture1Val_yaw) +
1) /
((float)FTM_SOURCE_CLOCK / 1000000);
//PRINTF("\r\nInput signals frequency = %f hz\r\n", 1/(pulseWidth_pitch*2)*1000000);
PRINTF("\r\nInput signals YAW pulse width = %f us\r\n", pulseWidth_yaw);
}
g_secondChannelOverflowCount_YAW = 0;
g_firstChannelOverflowCount_YAW = 0;

/* Enable first channel interrupt */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, FTM_FIRST_CHANNEL_INTERRUPT_ENABLE_YAW);

/* Enable second channel interrupt when the second edge is detected */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, FTM_SECOND_CHANNEL_INTERRUPT_ENABLE_YAW);

/* Enable overflow interrupt */
FTM_EnableInterrupts(DEMO_FTM_BASEADDR, kFTM_TimeOverflowInterruptEnable);
}
}

 

 

Additionally, could you please let me know what specific line of your code is the MCU halting?

Ans: Halting

erichsu_2-1619965272034.png

 

 

0 Kudos
Reply

5,182 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Eric,

I would recommend to try to implement this step by step, have you tried to change the example to use channel 0 and 1 before incrementing to 4 channels? If this work then it could be an issue of interrupt management, if this does not work then it could be a configuration issue.

Best regards,

Felipe

0 Kudos
Reply