FSL_USB_STACK problems with 10.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSL_USB_STACK problems with 10.6

1,690件の閲覧回数
arunkumar1989
Contributor I

Hello Everyone,

I am facing an unusual problem with the custom component created by Mr Erich Styger. Link -> FSL_USB_Stack

I am using a MK60FN1MOV with CW 10.6.

I am able to use the component normally,but when ever i close the project and re-open it again ,i get this error in the CDC component.

error.PNG.png

Its very frustrating to delete the "FSL_USB_STACK" components and again add it,whenever i open my project.

Is there a way around this?

Thanks in Advance

Arun

0 件の賞賛
返信
2 返答(返信)

1,546件の閲覧回数
BlackNight
NXP Employee
NXP Employee

This is a known bug/issue in Processor Expert, and shortly after that MCU10.6 update came out, a workaround has been added to the FSL_USB_Stack component.

That you see this problem let me think that you are not using the latest components.

Are you using the latest version from SourceForge (McuOnEclipse - Browse /PEx Components at SourceForge.net, latest release right now is from 27-Dec-2014).

See McuOnEclipse Releases on SourceForge | MCU on Eclipse how to download/install them.

I hope this helps,

Erich

1,546件の閲覧回数
arunkumar1989
Contributor I

Hello Erich,

Yes that did the trick, I downloaded the latest PEx components and now the CDC component module is not giving that error.

Thank you,

Arun

0 件の賞賛
返信