FSL AN4379 MSC bootloader for K20 fails on writing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSL AN4379 MSC bootloader for K20 fails on writing

1,231件の閲覧回数
kai_liu
Senior Contributor I

I have verified AN4379 MSC bootloader on FRDM-KL25Z successfully. https://community.freescale.com/docs/DOC-97782

Now I am doing the same thing on FRDM-K20D50M. The bootloader can enumerated on Windows XP. But saving S19 files failed.

So I put debug printf() in MSD_Event_Callback() of disk.c.

        printf("event=%02X",event);

        switch (event)

        case USB_APP_DATA_RECEIVED (0x4) -> br

        case USB_APP_SEND_COMPLETE (0x03) -> br

        case USB_MSC_START_STOP_EJECT_MEDIA -> br

        case USB_MSC_DEVICE_READ_REQUEST (0x81)

        case USB_MSC_DEVICE_WRITE_REQUEST (0x82)

        case USB_MSC_DEVICE_FORMAT_COMPLETE -> br

        case USB_MSC_DEVICE_REMOVAL_REQUEST (0x84)

        case USB_MSC_DEVICE_GET_INFO (0x85)

        default -> br

After sending file to bootloader, I found following log on terminal.

......

        event=03

        event=82

        offset=0x00000000,offset>>9=0x00000000

        event=84

        event=03   

The normal operation should be a sequence of event 0x82 (USB_MSC_DEVICE_WRITE_REQUEST ). But K20 firmware stops and host calls USB_MSC_DEVICE_REMOVAL_REQUEST later on.

The host reports Cannot copy K20_DEMO: The request could not be performaned because of an I/O device error.

K20_DEMO.S19 is a demo project with relocated address starts from 0x8000.

Any idea? Why host send USB_MSC_DEVICE_REMOVAL_REQUEST for which error?

ラベル(3)
タグ(2)
0 件の賞賛
返信
0 返答(返信)