FRDMK22 enable PEE mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDMK22 enable PEE mode

1,793 Views
claudiobrunelli
Contributor II

Hi.

I'd like to move my frdmk22 board, to PEE clock mode but I can't see different clock even changing values

in the below code.

Do I forget something ? Or ther's something wrong in my code ?

Thanks in advance...

Claudio

void PEE_InitMode(void)
{
    MCG->C2 = 0x2C;
    MCG->C1 = 0x98;
    while ((MCG->S & MCG_S_OSCINIT0_MASK) == 1)    ;    
    while ((MCG->S & MCG_S_IREFST_MASK) == 0);        
    while ((MCG->S & MCG_S_CLKST(10)) == 0x10);

    MCG->C5 = 0x03;  // /4
    MCG->C6 = 0x41;  // *25
    while ((MCG->S & MCG_S_PLLST_MASK) == 1);
    while ((MCG->S & MCG_S_LOCK0_MASK) == 1);

    MCG->C1 = 0x01;
    while ((MCG->S & MCG_S_CLKST(01)) == 0x01);

    SIM->SOPT2 |= SIM_SOPT2_PLLFLLSEL_MASK;
}

0 Kudos
Reply
3 Replies

1,668 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Claudio Brunelli,

   Enable the PEE mode need to follow this diagram.

pastedImage_1.png

I use the KDS PE create a project which is configuring the PEE mode,

pastedImage_2.png

I attach the project for your reference.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,668 Views
claudiobrunelli
Contributor II

Hi Kerry.

Sorry the delay in answering you. I prefer don't use PE. But I'm going to try your suggestion to use PE generated code. I will write soon as I can try.

Thanks.

Claudio

0 Kudos
Reply

1,668 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Claudio,

   PE code is just for your reference, you can don't use it, but just follow the code process write your own code.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply