FRDM board Eagle Footprint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM board Eagle Footprint

3,218 Views
aelma95
Contributor I

Hey guys, I'm find it very difficult to find eagle  foot print for the FRDM KE06z board. just wondering where can I find it or do i need to make one. I also need one for FRDM k64F. I need this as i'm designing a shield for both of them. 

0 Kudos
Reply
2 Replies

2,310 Views
haozh
Contributor I

Hello Robin,

Do you know where I can find the FRDM-K66F. I download the data on line, and it seems not the layout. It has the .DAT format.

Regards,

Hao

0 Kudos
Reply

2,310 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Abdelrahman,

Cadence OrCAD are available, you can download "Printed Circuit Board bill of materials and design files" from FRDM-KE06Z and FRDM-K64F.

This article shows how you can download Eagle CAD files for Kinetis: Freescale Kinetis CAD Footprints and Symbols for Eagle/Altium/etc | MCU on Eclipse

Hope that help. Have a nice day!

Best Regards,

Robin

0 Kudos
Reply