FRDM-Kx boards not in processor expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-Kx boards not in processor expert

1,473 Views
kevinangus
Contributor III

While having to go back to the drawing board for a 'lower' cost solution I looked at the KE0x and KL0x lines, I found support for the processors in Process Expert but the 'Board' support was not there:

FRDM-KE02Z40M

FRDM-KE02Z

FRDM-KL02Z

FRDM-KL03Z

FDRM-KL46Z

FRDM-K64F

I have the KL46Z and K64F but those are not supported in PE.

Any idea when the FRDM boards will be supported in PE?

The MKL02Z16VFK4 is high on my list as well as the MKL03Z16VFG4.

Thanks

0 Kudos
Reply
1 Reply

1,243 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

The only support for boards that Processor Expert adds is that it creates some components already configured for the boards.

For example, for the FRDM-KL25 there is a Red_LED component, that is basically a GPIO component with a custom name and the pin already configured to the one that is connected to the red pin of the RGB Led in the board.

But all the microcontrollers used in the boards you mention are already supported in Processor Expert, so you can begin to work with all the boards immediately.

Regards,


Santiago

0 Kudos
Reply