FRDM-KW40Z with Test Tool 12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW40Z with Test Tool 12

1,685件の閲覧回数
koonlee
Contributor I

I have a FRDM-KW40Z board and I would like to use Radio Test application in Test Tool 12.

First, I use Firmware Loaders to load "MAC 2003 ZTC 115200 KW24D512-USB ASP_RadioTest.srec".  I see "CMSIS-DAP MSD (E:\)" under the OpenSDA/J-Link List. When I click Upload button, I got the following error:

"Error: could not access MSD drive"

Did I miss any step?

Thanks for your help.

Koon

ラベル(2)
0 件の賞賛
返信
1 返信

1,338件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Koon,

Available images for Test tool are not compatible for KW40 MCU, as you can see, your image "MAC 2003 ZTC 115200 KW24D512-USB ASP_RadioTest.srec" is available for KW24D512 and not for KW40. So, you cannot use KW24's images to flash KW40 target.

Sorry for this inconvenience!

Regards,

Isaac Avila

0 件の賞賛
返信