FRDM-KW40 CMSIS DAP mbed interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KW40 CMSIS DAP mbed interface

2,158 Views
seanwu
Contributor V


Dear Sir,

I updated wrong firmware of CMSIS DAP mbed interface  on FRDM-KW40. It become PE OpenSDA interface.

Do you have the the CMSIS DAP interface firmware for FRDM-KW40?

Thanks.

BR,

Sean

Labels (1)
0 Kudos
Reply
3 Replies

1,830 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

KW40Z is Integrated MK22FN512VMP12 MCU.

FRDM-KW40Z is integrated with OpenSDA v2.1.

here is Default firmware application

CMSIS-DAP – kw40Z (binary)

here is Latest firmware application

does this answer your questions?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,830 Views
seanwu
Contributor V

Dear Sir,

   It works. Thanks for your help.

BR,

Sean

0 Kudos
Reply

1,830 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!


Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply