FRDM-KW24D512 OpenSDA not responding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW24D512 OpenSDA not responding

1,688件の閲覧回数
mattiastörnblad
Contributor II

Hi, after trying to update the OpenSDA firmware to jlink on FRDM-KW24D512 both OpenSDA and bootloader are not responding! Is it possible to unbrick it from another board?

ラベル(2)
0 件の賞賛
返信
1 返信

1,405件の閲覧回数
Wilgaced
Contributor II

Hi

I do the same with 3 units, so i can recovery thanks to Erich Styger (mcuoneclipce)

folow the step in this link, i use P&E multilink (the green) it work great.

https://mcuoneclipse.com/2014/11/10/recovering-the-frdm-k64f-bootloader-or-cloning-the-program-of-a-...

Note: i can recovery because i buy 4 units.

ok if you dont have other board here the link to memory dump

booloader_frdm-kw24D - Google Drive

0 件の賞賛
返信