FRDM-KL46Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL46Z

2,024件の閲覧回数
mattmabile
Contributor I

When i plug the FRDM-KL46Z into my Windows 8.1, 64-bit computer using the OpenSDA USB port the FRDM does not show up as a storage drive like the quick start manual says that it should.

0 件の賞賛
返信
2 返答(返信)

1,825件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matt,

This may be related with the bootloader and firmware version on you board, support for Windows 8/8.1 was added to Bootloader version 1.11 and MSD firmware version 1.14. Please make sure that your board is programmed with Bootloader version 1.11 or higher prior to attempting to update your OpenSDA board with a new firmware application.

You can find more information on how to perform the update and find out what version of Bootloader your board is programmed with on this link:

P&E Microcomputer Systems

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,825件の閲覧回数
mattmabile
Contributor I

Thanks Carlos. I update the firmware and it is working fine now.

Sent from my iPhone

0 件の賞賛
返信