FRDM-KL46Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL46Z

2,065 Views
mattmabile
Fresh Out Contributor

When i plug the FRDM-KL46Z into my Windows 8.1, 64-bit computer using the OpenSDA USB port the FRDM does not show up as a storage drive like the quick start manual says that it should.

0 Kudos
Reply
2 Replies

1,866 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matt,

This may be related with the bootloader and firmware version on you board, support for Windows 8/8.1 was added to Bootloader version 1.11 and MSD firmware version 1.14. Please make sure that your board is programmed with Bootloader version 1.11 or higher prior to attempting to update your OpenSDA board with a new firmware application.

You can find more information on how to perform the update and find out what version of Bootloader your board is programmed with on this link:

P&E Microcomputer Systems

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,866 Views
mattmabile
Fresh Out Contributor

Thanks Carlos. I update the firmware and it is working fine now.

Sent from my iPhone

0 Kudos
Reply