FRDM-KL46Z SLCD Details and Simulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL46Z SLCD Details and Simulation

2,509件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

I am presently porting some libraries from the K family to the KL family and just added SLCD support (on Freedom KL46Z board) and a simulation model for its SLCD. Fortunately the SLCD peripheral is fully compatible and so only the configuration and control of the LCD pins to the Luminex LCD-S401M16KR needed adjusting.


In the process I have added quite a lot of specific details about the configuration and operation for the Luminex LCD-S401M16KR on the FRDM-KL46Z to the following document which may be of interest to people who need to drive this SLCD as well as other types: http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf

This is an extension to K40 SLCD support as discussed in an old thread K40 Segment LCD - demo and simulation  which also shows the operation in a video.

Below is a screen shot of the uTasker simulator running a KL46 and the above SLCD - showing USB enumeration causing "USB" to be displayed on the SLCD.

Regards

Mark

FRDM-LK46Z.png

ラベル(1)
0 件の賞賛
返信
0 返答(返信)