FRDM-KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KL25Z

1,409 次查看
michalmarkus
Contributor I

hello, when i conect my FRDM-KL25Z, it isn't doing anything, demo isn't started. What can i do??

标签 (1)
0 项奖励
回复
2 回复数

1,349 次查看
pavel_krenek
NXP Employee
NXP Employee

It should be better if you more specified the issue (new board, or some application was programed)?

0 项奖励
回复

1,349 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Michal,

    Did you download the code to the FRDM-KL25 before?

  If you didn't download the code, and the board is not newly out of factory, it may have no response.

  Please download the KSDK2.0_FRDM-KL25,

  Click "build an sdk", then choose the board as FRDM-KL25 , generate the KSDK2.0  and download it.

  After you download it, please refer to the Getting Started with Kinetis SDK (KSDK) v.2.0.pdf in folder :SDK_2.0_FRDM-KL25Z\docs

  And download the sample code in folder: SDK_2.0_FRDM-KL25Z\boards\frdmkl25z, then check the function.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复